This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TDA4VM: Details/information about CPSW instances supported in J7 devices and software supported from TI SDK.

Part Number: TDA4VM
Other Parts Discussed in Thread: DRA829, , DRA821, TDA4VL, TDA4VH

Details/information about CPSW instances supported in J7 devices and software supported from TI SDK.

  • The following table will illustrate the different instances of CPSW supported in each of J7 device along with S/W support from TI SDK.

     

    S.No

    J7 Device

    MCU CPSW2G

    Main CPSW2G

    Main CPSW5G

    Main CPSW9G

    Main CPSW3G

    1

    J721E/TDA4VM/DRA829

    R: YES
    L: YES
    E: NO
    M: YES

    NA

    NA

    R: YES
    L: YES
    E: YES
    M: NO

    NA

    2

    J7200/DRA821

    R: YES
    L: YES
    E: NO
    M: YES

    NA

    R: YES
    L: YES
    E: YES
    M: NO

    NA

    NA

    3

    J721S2/TDA4VL

    R: YES
    L: YES
    E: NO
    M: YES

    R: YES
    L: YES
    E: NO
    M: NO

    NA

    NA

    NA

    4

    J784S4/TDA4VH

    R: YES
    L: YES
    E: NO
    M: YES

    R: YES
    L: YES
    E: NO
    M: NO

    NA

    R: YES
    L: YES
    E: YES
    M: NO

    NA

    5

    J722S/J7AEN

    NA

    NA

    NA

    NA

    R: NO
    L: YES
    E: NO
    M: YES

    R: RTOS Enet Example
    L: Native Linux Driver
    E: RTOS EthFw Application
    M: MCAL Eth Driver
    NA: Not Applicable (CPSW instance is not supported in respective SoC)

    Note:
    We can’t use multiple applications at the same time for any of the CPSW instances. Only one of the above can be used.

    Interface Supported from CPSW Instances:

    S.No

    CPSW Instance\ Interface

    RGMII/RMII

    SGMII

    XAUI (2.5G SGMII)

    QSGMII

    USXGMII/XFI
    (5G/10G)

    1

    MCU CPSW2G

    YES

    -

    -

    -

    -

    2

    Main CPSW2G

    YES

    -

    -

    -

    -

    3

    Main CPSW5G

    YES

    YES

    YES

    YES

    YES (Only from Port-1)

    4

    Main CPSW9G (J721E)

    YES

    YES

    YES

    YES

    YES (Only from Port-1, Port-2)

    5

    Main CPSW9G (J784S4)

    -

    YES

    YES

    YES

    YES (Only from Port-1, Port-2)

    6

    Main CPSW3G

    YES

    YES

    -

    -

    -


    Note:
    Only one interface can be used at a time, we can’t enable multiple interfaces at the same time.

    CPSWnG: Has one Internal Host Port + (n-1) External Physical Port for connecting to the External world.