Part Number: TMDS64EVM
Tool/software:
Hi
I have a peace of code for DCC0 peripheral and I want to test it by changing SYSCLK frequency. If I understand correctly after changing frequency ESM interrupt should be triggered. I tried play with that by /sys/devices/system/cpu/cpufreq/ but unfortunately this directory is empty. Also I tried to this with k3conf tool by typing command k3conf set clock 16 6 25000000 but frequency stays the same as before. According to the documentation, the clock source DEV_DCC0_DCC_CLKSRC6_CLK represents Main Sysclk0. This SYSCLK0 is CPU frequency at which Linux OS is running, if I understood correctly.
root@puma:~# k3conf set clock 16 6 25000000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-88-g982f5c2 built Mon Nov 4 11:02:54 AM UTC 2024) |
| SoC | AM64x SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.4--v08.06.04 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
|-------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|-------------------------------------------------------------------------------------|
| 16 | 0 | DEV_DCC0_DCC_CLKSRC0_CLK | CLK_STATE_READY | 200000000 |
| 16 | 1 | DEV_DCC0_DCC_CLKSRC1_CLK | CLK_STATE_READY | 80000000 |
| 16 | 2 | DEV_DCC0_DCC_CLKSRC2_CLK | CLK_STATE_READY | 133333333 |
| 16 | 3 | DEV_DCC0_DCC_CLKSRC3_CLK | CLK_STATE_READY | 250000000 |
| 16 | 4 | DEV_DCC0_DCC_CLKSRC4_CLK | CLK_STATE_READY | 25000000 |
| 16 | 5 | DEV_DCC0_DCC_CLKSRC5_CLK | CLK_STATE_READY | 0 |
| 16 | 6 | DEV_DCC0_DCC_CLKSRC6_CLK | CLK_STATE_READY | 500000000 |
| 16 | 7 | DEV_DCC0_DCC_CLKSRC7_CLK | CLK_STATE_READY | 60000000 |
| 16 | 8 | DEV_DCC0_DCC_INPUT00_CLK | CLK_STATE_READY | 25000000 |
| 16 | 9 | DEV_DCC0_DCC_INPUT01_CLK | CLK_STATE_READY | 0 |
| 16 | 10 | DEV_DCC0_DCC_INPUT02_CLK | CLK_STATE_READY | 12500000 |
| 16 | 11 | DEV_DCC0_DCC_INPUT10_CLK | CLK_STATE_READY | 250000000 |
| 16 | 12 | DEV_DCC0_VBUS_CLK | CLK_STATE_READY | 125000000 |
|-------------------------------------------------------------------------------------|