Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Hi E2E'rs
We are developing an interface between Actel Igloo FPGA and OMAPL138.
An apps note from Xilinx details a 16-bit asynchronous interface which is used as a baseline for our design { "Interfacing Xilinx FPGAs to TI DSP Platforms Using the EMIF" (xapp753.pdf pg 18)}. The FPGA is configured as a FIFO in this instance and therefore only the Data lines are pysically attached to the FPGA.
1: If we use this interface can the multiplexed pin functions attached to the EMIF address lines be used for another interface simultaneously (In particular we are thinking of MMCSD0 interface)?
Guess what I am effectively asking is can the EMIF be operated
a - generating the usual write/read/output enables and chip select's
b- without toggeling the address lines
c- whilst the MMCSD card is also enabled on the interface.
2: We have searched high and low for an example of a similar interface to an Actel Igloo device being interfaced to a c64x or OMAPL138 without success.
Seems like there is too little info out there - is there a reason for that ie are there any "gotcha's" we should know about Actel FPGA interfacing to OMAPL138's ?
BR
Barry