This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VP-Q1: Authenticate in place (Secure boot)

Part Number: TDA4VP-Q1


Tool/software:

Hello TI support team,

Using SDK v10.00.00.08, We are trying to achieve secure boot using the SBL. There have some points that are needed to be clarified.

1. In the security x509 certificate extension 'System Firmware Load Extension', what is meant by the attribute auth_in_place ? Does it authenticate in place in flash device (NOR) ? 

2. Using the API 'Sciclient_procBootAuthAndStart' to be able to authenticate, start and boot, What are the required extensions in x509 certificate ? 

3. Is there any example for running an application XIP (Image, booting) ?

Thanks,
Omar