Other Parts Discussed in Thread: UCD9244, UCD9222, UCD9224
Hi All,
I have just come unstuck. I was going to use a UCD9244 for the four C6678 rails (CVDD, 1V0, 1V5, 1V8).
However, despite the UCD9244 datasheet saying "Supports Voltage Margining & Sequencing", I have been informed that it's sequencing options are very limited. It can only sequence automatically using a time delay i.e. it cannot delay power up of Rail #2 until Rail #1 is stable. Also, as I understand it, it won't monitor Rail #1 and prevent Rail #2 from powering up if Rail #1 fails.
My reading of the C6678 power sequencing is that we need to monitor the rails in the sequence and that a time delayed power up sequence isn't good enough.
It looks to me like the UCD9244 is only good for the Smart Reflex CVDD when you have four C6678 DSP's on the board, and that you can't use it for any of the other rails.
Richard