Could I use the EMIF16 as interface for two flash memories, one for datalogging and the other as boot flash, or this can slow down the DSP?
The access in the boot flash is required only one time, after the power-on, or even after this period?
In other words, could happends that the datalogging process, in progress on one flash memory, halts the access in the boot flash, causing the stop of the system?
Thanks in advance