Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TDA4VL-Q1: Recommendations for testing ECC error injection

Part Number: TDA4VL-Q1

Tool/software:

At what stage must ECC error injection be tested? Should it be tested at startup or can it be tested at runtime?

  • Hi,

    The following are the general recommendations on when the error injection on ECC aggregators must be performed:

    • The ECC error injection and monitoring of the error response should be run at ‘startup’ where possible.
    • An alternative recommended approach is to run ECC error injection at ‘shutdown’.

    When running of ECC error injection during ‘runtime’, the system integrator must be aware of the below:

    For interconnect endpoints:

    • The ECC SEC error injection runs during idle cycles, so can be run during ‘runtime’ for checkers of all types.
      • Parity and redundant bit error injections are non-destructive and can be done at runtime.
    • The ECC DED error injection runs during idle cycles, so can be run during ‘runtime’.
      • Only single bit error injections are to be done on parity/redundant checker types. This is because these protect odd number of injections. A 2 bit injection on parity will not cause a failure.

    For RAM memories:

    • ECC self-test for SEC on RAM memories, can be run at runtime:
      • The ECC self-test for SEC injects a single-bit error that is corrected in-line.
    • ECC DED error injection during ‘runtime’ for RAM memories, should only be done for memories with direct read access
      • Two examples of direct read access memories are MSMC SRAM and MCU SRAM
      • Double-bit error injection on all other embedded SRAMS could possibly result in the downstream IP reading bad data if run during ‘runtime’
    • ECC error injection on inject-only memories, should be run at ‘startup’, they are not recommended to be run during ‘runtime’.

    Regards,

    Josiitaa