Other Parts Discussed in Thread: SYSBIOS
Hi,
I have the error in the post: http://e2e.ti.com/support/embedded/f/355/p/139836/504786.aspx. Hardware is the Mistral 8148, the build is my own executable, that was working (doing nothing with one task) earlier in the week, ... but I don't know when it started. I upgraded from CCS5.1.0.07001 to CCS5.1.0.08020 yesterday. I've also changed from BIOS 6.32.4.49 to 6.32.5.54.
I don't see these lines in the former post:
var
Timer = xdc.useModule(‘ti.sysbios.timers.dmtimer.Timer’);
Timer.checkFrequency = false;
in my .cfg file source, am I looking in the wrong place?
I do create a timer in my code, like this:
Clock_Params_init(&clkParams);
clkParams.period = 5;
clkParams.startFlag = TRUE;
Clock_create((ti_sysbios_knl_Clock_FuncPtr)softTimer_1mS, 5, &clkParams, NULL);
Clock_start(soft_1ms);
This is what I get when I 'load' the program, 3 separate loads (doesn't let me run when it finishes - points to Abort()).
[C674X_0] ti.sysbios.timers.dmtimer.Timer: line 1031: E_freqMismatch: Frequency mismatch: Expected 32768 Hz, actual: 761421 Hz
xdc.runtime.Error.raise: terminating execution
[C674X_0] ti.sysbios.timers.dmtimer.Timer: line 1039: E_freqMismatch: Frequency mismatch: Expected 32768 Hz, actual: 908900 Hz. You need to modify Timer.intFreq.lo to match the actual frequency.
xdc.runtime.Error.raise: terminating execution
[C674X_0] ti.sysbios.timers.dmtimer.Timer: line 1039: E_freqMismatch: Frequency mismatch: Expected 32768 Hz, actual: 367262 Hz. You need to modify Timer.intFreq.lo to match the actual frequency.
xdc.runtime.Error.raise: terminating execution
Any ideas what happened?
Thanks,
Matt