Part Number: AM3357
Tool/software:
Hi,
I would like you to confirm about below.
* When we use MII interface with emac, is there any specific internal pull up/pull down setting for each pins ?
BR,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3357
Tool/software:
Hi,
I would like you to confirm about below.
* When we use MII interface with emac, is there any specific internal pull up/pull down setting for each pins ?
BR,
Hello Ryuuichi machida
Thank you.
For the MAC interface operation, i do not see the need for any pulls.
When the MAC interfaces to a EPHY, the need for parallel termination is EPHY dependent.
Regards,
Sreenivasa
Hi Sreenivasa,
Thank you for your reply.
>For the MAC interface operation, i do not see the need for any pulls.
I could not undertand above case. Which case will be applied above ?
>When the MAC interfaces to a EPHY, the need for parallel termination is EPHY dependent.
Do you mean that we should perform same setting as Ethernet PHY ?
BR,
Hello Ryuuichi machida
For the MAC interface operation, i do not see the need for any pulls.
I could not undertand above case. Which case will be applied above ?
The MAC interface pulls have EPHY dependency.
The idea is to ensure processor IOs or the attached device IOs do not float.
Regards,
Sreenivasa