This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: DDR frequency use 1866MHz.

Part Number: AM62A7
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hello,team

Our product needs to increase the bandwidth of the DDR to improve performance, and we use TI Sysconfig to configure the 1866MHz file.

Then start the sitara with the boot process of tiboot3, at this time, the boot is normal, and no problem is found in the operation, but the boot process using the sbl_stage1 cannot be started, why is this?

Also, are there any risks if we run 1866MHz with the chip below?

Best regards,
XUE Fadong
  • Please check table 10-1 in the datasheet for the capabilities of your device.  It appears you have a device which can only operate the memory at 3200MTS (1600MHz)

    Regards,

    James