Tool/software:
Hi Experts,
Our SDK is TDA4VE SDK9.2. We compile the valgrind(an open source memory check tool) on the TDA4VE board and run it, then it report the error log as follow:
------------------------------
==1639== Memcheck, a memory error detector
==1639== Copyright (C) 2002-2024, and GNU GPL'd, by Julian Seward et al.
==1639== Using Valgrind-3.24.0 and LibVEX; rerun with -h for copyright info
==1639== Command: ls
==1639==
valgrind: Fatal error at startup: a function redirection
valgrind: which is mandatory for this platform-tool combination
valgrind: cannot be set up. Details of the redirection are:
valgrind:
valgrind: A must-be-redirected function
valgrind: whose name matches the pattern: strlen
valgrind: in an object with soname matching: ld-linux-aarch64.so.1
valgrind: was not found whilst processing
valgrind: symbols from the object with soname: ld-linux-aarch64.so.1
valgrind:
valgrind: Possible fixes: (1, short term): install glibc's debuginfo
valgrind: package on this machine. (2, longer term): ask the packagers
valgrind: for your Linux distribution to please in future ship a non-
valgrind: stripped ld.so (or whatever the dynamic linker .so is called)
valgrind: that exports the above-named function using the standard
valgrind: calling conventions for this platform. The package you need
valgrind: to install for fix (1) is called
valgrind:
valgrind: On Debian, Ubuntu: libc6-dbg
valgrind: On SuSE, openSuSE, Fedora, RHEL: glibc-debuginfo
valgrind:
valgrind: Note that if you are debugging a 32 bit process on a
valgrind: 64 bit system, you will need a corresponding 32 bit debuginfo
valgrind: package (e.g. libc6-dbg:i386).
valgrind:
valgrind: Cannot continue -- exiting now. Sorry.
------------------------------
As the log metioned, we need an non-stipped ld-linux-aarch64.so.1 library. So could you provide the non-stipped ld-linux-aarch64.so.1 please?
Best Regards
Hawayi