This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM69: Logic level for USB0_ID pin

Part Number: AM69

Tool/software:

Hi,

There seems to be some conflicting information about the logic level for the USB0_ID pin on the AM69 processor. In the AM69 datasheet Table 5-1, pin USB0_ID (ALY package: AN17) is listed with an I/O Voltage of 3.3V. However, the power column in that same table lists VDDA_0P8_ USB / VDDA_1P8_ USB / VDDA_3P3_ USB. Furthermore, in the SK-AM69 evaluation kit schematic, the power supply for the AN17 pin seems to be connected to VDDA_0P8_USB, which is in turn connected to VDD_CORE_0V8. 

What is the logic level for the USB0_ID pin? Is it required to be 3.3V, or can it be 0.8V or 1.8V?

Thanks for your help.