TDA4AP-Q1: DC, AC parameters for Reference clock inputs SERDES0 to SERDES4

Part Number: TDA4AP-Q1

Tool/software:

Hello,

from the TDA4 datasheet Table 6-2 there is only one parameter given. Can you please provide more information about:
single ended crossing voltage area (min, max)
absolute voltage range for p/n signals
required rise and fall times and duty cycle range
Delta cross point voltage

Thanks for your answer in advance.

  • Thomas,

    The ref clk complies with the electrical parameters specified in PCI Express® Base Specification Revision 4.0. If the ref clk is used as an input, table 6-2 is in addition to the specs.