TDA4VE-Q1: How to implement Vector boot-manager with TIFS

Part Number: TDA4VE-Q1

Tool/software:

Dear champs,

The vector Bootmanager package contains a few libraries from TI, but they don’t provide the routines needed for booting via TIFS. We are looking for information from TI for the proper way to implement (secure) boot via TIFS / SCI client.

  • What is the intended routine to trigger a start of a multicore image with certificate via TIFS / SCI ?
    • SBL_BootImage ? SBL_OSPIBootImage ? SBL_MulticoreImageParse?
    • For HSM : SBL_loadAndAuthHsmBinary
  • Why is this routine not present in the Vector Bootmanager and its TI libs?
  • How can we change the Vector Bootmanager so that this routine can be used?

Thanks and kind regards, one and zero

  • Hi,

    TI does not have any information on Vector BootManager code, it is not a TI deliverable. Please reach out to Vector for support regarding Vector BootManager.

    If there are questions w.r.t SBL or the Boot App reference code provided in the TI RTOS SDK, then we can help answer the questions.

    regards

    Suman