This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM644x UART NAND boot

Hello everyone,

I am trying to flash U-Boot on my DV644x DVEVM board. It's revision F. I donot have JTAG emulator so i am trying to use the UART boot feature.

I have all latest flashing software

1). DM644x_FlashAndBootUtils_1_10

2). DM644x_FlashAndBootUtils_1_50

3). DM644x_FlashAndBootUtils_2.00

and also DVFlasher_1_10.exe


I have set the CS2( J4 ) jumper to NAND,

In my case the J4 has options for -    FLASH, SRAM, NAND & DC

The S3 dip switches are set to select uart boot mode 1100111110

My problem is i cannot seem to flash U-boot with any of the above mentioned software.

I can erase the NAND flash with DVFlasher_1_10.exe  but can't seem to FLASH U-Boot with it. Here is the console output..

-----------------------------------------------------

   TI DVFlasher Host Program for DM644x

   (C) 2007, Texas Instruments, Inc.

-----------------------------------------------------

Platform is Windows.

Flashing NAND with u-boot-567-nand.bin.


Attempting to connect to device COM1...

Press any key to end this program at any time.

Waiting for DVEVM...

BOOTME commmand received. Returning ACK and header...

ACK command sent. Waiting for BEGIN command...

        DVEVM:    BEGIN

BEGIN commmand received. Sending CRC table...

CRC table sent.  Waiting for DONE...

DONE received.  Sending the UART UBL file...

DONE received.  UART UBL file was accepted.

UART UBL Transmitted successfully.

 

        DVEVM:  TI UBL Version: 1.00, Flash type: NAND

        DVEVM:  Booting PSP Boot Loader

        DVEVM:  PSPBootMode = UART

 

Waiting for UBL on DVEVM...

UBL's BOOTPSP commmand received. Returning CMD and command

CMD value sent.

SENDUBL received. Returning ACK and header for UBL data...

ACK command sent. Waiting for BEGIN command...

UART UBL's BEGIN commmand received. Sending the Flash UBL

Flash UBL code sent.  Waiting for DONE...

DONE received.  All bytes of Flash UBL code received...

  Nothing Happens after this..

 

So I tried the other software, DM644x_FlashAndBootUtils_1_10

But with this i cant even erase the NAND flash and the board seems to restart and stars giving the BOOTME prompt.. here is the console output..

-----------------------------------------------------

   TI Serial Flasher Host Program for DM644x

   (C) 2008, Texas Instruments, Inc.

   Ver. 1.10

-----------------------------------------------------

Platform is Windows.

Globally erasing NAND flash.

 

Attempting to connect to device COM1...

Press any key to end this program at any time.

 

Waiting for the DM644x...

BOOTME commmand received. Returning ACK and header...

ACK command sent. Waiting for BEGIN command...

        Target:   BEGIN

BEGIN commmand received. Sending CRC table...

CRC table sent.  Waiting for DONE...

DONE received.  Sending the UBL...

DONE received.  UBL was accepted.

UBL transmitted successfully.

 

        Target: Chip initialization passed!

        Target: TI SFT Version: 1.10

        Target: Booting Catalog Boot Loader

        Target: BootMode = UART

 

Waiting for SFT on the DM644x...

        Target: Starting UART Boot...

        Target: BOOTUBL

BOOTUBL commmand received. Returning CMD and command...

CMD value sent.  Waiting for DONE...

        Target:    DONE

DONE received. Command was accepted.

        Target: NAND_open() failed!Starting UART Boot...

        Target: BOOTUBL

 

Waiting for SFT on the DM644x...

        Target: Starting UART Boot...

        Target: BOOTUBL

BOOTUBL commmand received. Returning CMD and command...

CMD value sent.  Waiting for DONE...

        Target:    DONE

DONE received. Command was accepted.

        Target:  BOOTME

        Target:  BOOTME

        Target:  BOOTME

        Target:  BOOTME

        Target:  BOOTME

        Target:  BOOTME

 

 

Next, i tried the software DM644x_FlashAndBootUtils_1_50..This also seems to restart..here is the console output..

-----------------------------------------------------

   TI Serial Flasher Host Program for DM644x

   (C) 2009, Texas Instruments, Inc.

   Ver. 1.50

-----------------------------------------------------

Platform is Windows.

Globally erasing NAND flash.

 

Attempting to connect to device COM1...

Press any key to end this program at any time.

 

 

Waiting for the DM644x...

BOOTME commmand received. Returning ACK and header...

ACK command sent. Waiting for BEGIN command...

        Target:   BEGIN

BEGIN commmand received. Sending CRC table...

 100% [                                                              ]

                           CRC table sent....

 

 

 

Waiting for DONE...

DONE received.  Sending the UBL...

 100% [                                                              ]

                              UBL sent....

 

 

DONE received.  UBL was accepted.

UBL transmitted successfully.

 

 

Waiting for SFT on the DM644x...

        Target: Starting UART Boot...

        Target: BOOTUBL

BOOTUBL commmand received. Returning CMD and command...

CMD value sent.  Waiting for DONE...

        Target:    DONE

DONE received. Command was accepted.

        Target:  BOOTME

        Target:  BOOTME

        Target:  BOOTME

        Target:  BOOTME

 

 

Next, I tried with the software DM644x_FlashAndBootUtils_2_00 But in this case it hangs at..

 

Waiting for SFT on the DM644x…

 

 

 

 

Can anybody help me with the same. I hope i am doing everything right.

 

Thanking you in advance..

Joydeep