This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VEN-Q1: What is the anticipated production life cycle

Part Number: TDA4VEN-Q1
Other Parts Discussed in Thread: TDA4AEN-Q1,

Tool/software:

What is the anticipated production life cycle for the TDA4VEN-Q1 and TDA4AEN-Q1?

Are the two parts interchangeable (i.e. one can be an alternate of the other)?

  • Hello,  

    The production life cycle is >10 years.  Yes the two parts are pin compatible and can be interchanged from a hardware perspective.  The feature set of the two parts are slightly different and is highlighted in the data manual.

    Regards,

    Kyle