Other Parts Discussed in Thread: OMAPL138, OMAP-L137
Hi,
I want to use DSP/LINK to allow communication between an existing DSP/BIOS project running on the C6748 core of an OMAPL138 and the ARM on the same device. My project has been built and tested using CCS 4.2. I have downloaded the dsplink_linux_1_65_00_03 package which contains the source for the DSP/LINK libraries. The user guide details how to build these using gmake, but can these be built using CCS? Do any CCS projects or even pre-built libraries exist anywhere?
Cheers,
John