This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62P: Is MPEG2 encoding possible with AM62P?

Genius 3215 points

Part Number: AM62P
Other Parts Discussed in Thread: TMS320DM365

Tool/software:

Hi All,

My client is looking for a device that can encode MPEG2.

Is MPEG2 encoding possible with AM62P?

However, the TMS320DM365 and other devices are more than 10 years old,
Even if I were to develop a device with this, it would likely be EOL soon.

Attached is a comparison chart I dropped from TI's document.
TMS320DM816x series and others are also capable of MPEG2 encoding.
The TMS320DM816x series is also capable of MPEG2 encoding.
Is it possible to use this one for a long time?

The target is currently realized with a different SoC.

(1) H.264 system
Video
 Compression method: H.264
 Resolution: 1080i 29.97
 Profile: HP@L4 or higher
 Bit rate: 2Mbps to 12Mbps
 Resolution: NTSC
 Profile: MP@L3 or higher
 Bit rate: 128 kbps to 2 Mbps
Audio
 Compression method:MPEG-2 AAC
 Bit rate: 64 kbps to 128 kbps
Multiplexing system
 MPEG2 TTS

(2) MPEG2 system
Video
 Compression system: MPEG2
 Resolution: NTSC
 Profile: MP@ML
 Bit rate: 1.5Mbps to 6Mbps
Audio
 Compression method: MPEG-1 Layer 2
Multiplexing system
 MPEG2 PS
Is.

Please tell us about TI's current series development and whether MPEG2 compression is possible.

Also, please let us know if you have a product that can compress MPEG2 up to HD.

Best Regards,

Ito