This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AH-Q1: spi-nor configuration

Part Number: TDA4AH-Q1

Tool/software:

Hi,

   I've try to configure the nor-spi on sdk 10 version, compiling using yocto,

  here is my dts node: (u-boot dts)

&ospi0 {
        bootph-all;
        status = "okay";
        pinctrl-names = "default";
        pinctrl-0 = <&mcu_fss0_ospi0_pins_default>, <&mcu_fss0_ospi0_1_pins_default>;

        ospi0_nor: flash@0 {
                status = "okay";
                compatible = "jedec,spi-nor";
                reg = <0>;
                spi-max-frequency = <25000000>;
                spi-tx-bus-width = <8>;
                spi-rx-bus-width = <8>;
                cdns,tshsl-ns = <10>;
                cdns,tsd2d-ns = <30>;
                cdns,tchsh-ns = <2>;
                cdns,tslch-ns = <2>;
                cdns,read-delay = <4>;

                partitions {
                        compatible = "fixed-partitions";
                        #address-cells = <1>;
                        #size-cells = <1>;

                        partition@0 {
                                label = "ospi.tiboot3";
                                reg = <0x0 0x80000>;
                        };

                        partition@80000 {
                                label = "ospi.tispl";
                                reg = <0x80000 0x200000>;
                        };

                        partition@280000 {
                                label = "ospi.u-boot";
                                reg = <0x280000 0x400000>;
                        };

                        partition@680000 {
                                label = "ospi.env";
                                reg = <0x680000 0x40000>;
                        };

                        partition@6c0000 {
                                label = "ospi.env.backup";
                                reg = <0x6c0000 0x40000>;
                        };

                        partition@800000 {
                                label = "ospi.rootfs";
                                reg = <0x800000 0x37c0000>;
                        };

                        partition@3fc0000 {
                                bootph-all;
                                label = "ospi.phypattern";
                                reg = <0x3fc0000 0x40000>;
                        };
                };
        };
};

But, it doesn't work, I'm getting following error while try to probe from U-boot CLI

Hit any key to stop autoboot:  0
=>
=>
=>
=>
=>
=> sf
sf - SPI flash sub-system

Usage:
sf probe [[bus:]cs] [hz] [mode] - init flash device on given SPI bus
                                  and chip select
sf read addr offset|partition len       - read `len' bytes starting at
                                          `offset' or from start of mtd
                                          `partition'to memory at `addr'
sf write addr offset|partition len      - write `len' bytes from memory
                                          at `addr' to flash at `offset'
                                          or to start of mtd `partition'
sf erase offset|partition [+]len        - erase `len' bytes from `offset'
                                          or from start of mtd `partition'
                                         `+len' round up `len' to block size
sf update addr offset|partition len     - erase and write `len' bytes from memory
                                          at `addr' to flash at `offset'
                                          or to start of mtd `partition'
sf protect lock/unlock sector len       - protect/unprotect 'len' bytes starting
                                          at address 'sector'
=> sf probe
Error: subnode with SPI flash config missing!
Invalid bus 0 (err=-19)
"Synchronous Abort" handler, esr 0x96000021, far 0x4a
elr: 00000000808350dc lr : 000000008081fd64 (reloc)
elr: 00000000fff230dc lr : 00000000fff0dd64
x0 : 0000000000000002 x1 : 0000000000000000
x2 : 000000000000000a x3 : 0000000042300000
x4 : 0000000042300000 x5 : 00000000fde899dc
x6 : 0000000000000039 x7 : 00000000fde89e70
x8 : 0000000000000001 x9 : 00000000ffffffd8
x10: 000000000000000d x11: 0000000000000006
x12: 00000000fde89d9c x13: 00000000fde8a290
x14: 00000000fffffffe x15: 00000000fde899dc
x16: 00000000fff4bfe8 x17: 0000000000000000
x18: 00000000fdeaddb0 x19: 0000000000000000
x20: 0000000000000000 x21: 0000000000000000
x22: 0000000000000000 x23: 00000000017d7840
x24: 00000000ffffffed x25: 0000000000000001
x26: 00000000fffe7000 x27: 0000000000000000
x28: 00000000fdeb6700 x29: 00000000fde89ef0

Code: b4000040 f9401c00 d65f03c0 b4000040 (f9402400)
Resetting CPU ...

from this my understanding is, the sub node which is related to spi-nor is missing 
could you help me on this?