Other Parts Discussed in Thread: OMAPL138
Hello,
I'm very excited to find OMAPL138_StarterWare, it's exactly what I've been after for quite sometime.
So, I downloaded CodeSourcery Lite 2009q1 as it includes GCC4.33 used in this package.
I'm using the latest Cygwin, probably released 2006 ?.
I failed to compile the example UART.
So I clean required libraries and try to re-compile to see if I'm ab;le to. Those libraries are : drivers, platform, system_config, ipclite, utils, usblib, grlib, nandlib.
It appears I'm able to re-compile all of them successfully.
The error relates to system LIBC and LIBGCC.
Your help is greatly appreciated.
Thanks,
Duy-Ky
Below is capture of make process
$ make clean; make all
========================= Debug LPATH -L/cygdrive/c/SW_DEV/CodeSourcery/CSL_2009q1/arm-none-eabi/lib/ -L/cygdrive/c/SW_DEV/CodeSourcery/CSL_2009q1/lib/gcc/arm-none-eabi/4.3.3/ -L../../../../../..//bin
ary/armv5/gcc/omapl138/drivers/ -L../../../../../..//binary/armv5/gcc/omapl138/evmOMAPL138/platform/ -L../../../../../..//binary/armv5/gcc/omapl138/system_config/ -L../../../../../..//binary/armv5/gcc
/omapl138/ipclite/ -L../../../../../..//binary/armv5/gcc/utils/ -L../../../../../..//binary/armv5/gcc/omapl138/usblib/ -L../../../../../..//binary/armv5/gcc/grlib/ -L../../../../../..//binary/armv5/gc
c/nandlib/ =========================
make TARGET_MODE=debug lib
make[1]: Entering directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/evmOMAPL138/uart'
make[2]: Entering directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/drivers'
make[2]: `debug' is up to date.
make[2]: Leaving directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/drivers'
make[2]: Entering directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/evmOMAPL138/platform'
make[2]: `debug' is up to date.
make[2]: Leaving directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/evmOMAPL138/platform'
make[2]: Entering directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/system_config'
make[2]: `debug' is up to date.
make[2]: Leaving directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/system_config'
make[2]: Entering directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/utils'
make[2]: `debug' is up to date.
make[2]: Leaving directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/utils'
========================= LIB =========================
make[1]: Leaving directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/evmOMAPL138/uart'
make TARGET_MODE=Debug bin
make[1]: Entering directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/evmOMAPL138/uart'
========================= BIN LPATH -L/cygdrive/c/SW_DEV/CodeSourcery/CSL_2009q1/arm-none-eabi/lib/ -L/cygdrive/c/SW_DEV/CodeSourcery/CSL_2009q1/lib/gcc/arm-none-eabi/4.3.3/ -L../../../../../..//binar
y/armv5/gcc/omapl138/drivers/Debug -L../../../../../..//binary/armv5/gcc/omapl138/evmOMAPL138/platform/Debug -L../../../../../..//binary/armv5/gcc/omapl138/system_config/Debug -L../../../../../..//bin
ary/armv5/gcc/omapl138/ipclite/Debug -L../../../../../..//binary/armv5/gcc/utils/Debug -L../../../../../..//binary/armv5/gcc/omapl138/usblib/Debug -L../../../../../..//binary/armv5/gcc/grlib/Debug -L.
./../../../../..//binary/armv5/gcc/nandlib/Debug =========================
arm-none-eabi-gcc -c -g -fdata-sections -ffunction-sections -Wall -I../../../../../..//include -I../../../../../..//include/hw -I../../../../../..//include/armv5 -I../../../../../..//include/armv5/om
apl138 -I../../../../../..//grlib/include -I../../../../../..//usblib/include -I../../../../../..//ipclite/include -I../../../../../..//nandlib/include -I"/cygdrive/c/SW_DEV/CodeSourcery/CSL_2009q1/in
clude" -Domapl138 -DevmOMAPL138 ../../../../../../examples/evmOMAPL138/uart//*.c
arm-none-eabi-ld -e Entry -u Entry -u __aeabi_uidiv -u __aeabi_idiv --gc-sections -L"/cygdrive/c/SW_DEV/CodeSourcery/CSL_2009q1/arm-none-eabi/lib/" -L"/cygdrive/c/SW_DEV/CodeSourcery/CSL_2009q1/lib/gc
c/arm-none-eabi/4.3.3/" -L../../../../../..//binary/armv5/gcc/omapl138/drivers/Debug -L../../../../../..//binary/armv5/gcc/omapl138/evmOMAPL138/platform/Debug -L../../../../../..//binary/armv5/gcc/oma
pl138/system_config/Debug -L../../../../../..//binary/armv5/gcc/omapl138/ipclite/Debug -L../../../../../..//binary/armv5/gcc/utils/Debug -L../../../../../..//binary/armv5/gcc/omapl138/usblib/Debug -L.
./../../../../..//binary/armv5/gcc/grlib/Debug -L../../../../../..//binary/armv5/gcc/nandlib/Debug -o Debug/uartEcho.out -Map Debug/uartEcho.map \
Debug/*.o* -T uartEcho.lds -ldrivers -lutils -lplatform -lsystem_config -lc -lgcc
C:\SW_DEV\CodeSourcery\CSL_2009q1\bin\arm-none-eabi-ld.exe: cannot find -lc
make[1]: *** [bin] Error 1
make[1]: Leaving directory `/home/Duy-Ky/OMAPL138_StarterWare_1_10_01_01/build/armv5/gcc/omapl138/evmOMAPL138/uart'
make: *** [debug] Error 2
$