This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: Processor selection

Part Number: PROCESSOR-SDK-AM335X

Tool/software:

I am looking for a Processor which will either work on 32-bit Linux or 32-bit windows with following specification

  1. The Processor should have reference code associated with it.
  2. It should work on either 32-bit Linux or 32-bit windows OS.
  3. The processor should have following interfaces
  • 10/100 Ethernet
  • USB Type-C
  • DDR3/DDR4 SDRAM
  • NOR Flash
  • VGA or HDMI Port