This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GIO0 not latched at reset (DM365)

According to sprufg5a, GIO0 pin's state is latched at reset and could be read from BOOTCFG register bit GIO0_RESET. That doesn't seem to work on my h/w, always reads 0. Reading the state of this pin (once the code starts running) shows a 1, oscilloscope confirms that it's at logic high when reset pulse goes high.

Are there any limitations to this feature, like only certain boot modes that it works with?