Other Parts Discussed in Thread: TLV320AIC33
Audio Example on DM648
Hello
We are trying to work with the audio example in the DM648 .
The project example name is AUDIO_GIO which located under the Examples directory .
This example is receiving Audio via the line in input of the 648 EVM and sending the Audio
output to the Speakers via the Line out mini RCA connector .
My question is ,what kind of digital audio format exist in this code after the signal is
sampled and put in a memory buffer ?
The input codec is AIC33 chip which is not doing any compression to the signal (as far as I
know ) .So it means that synthetic normal audio , from outside file can be played .
Is that correct ?
Can I use simple raw audio data from the type of A low , U low or PCM uncompressed ?
I want to create an audio file by outside PC SW and use the audio data of this file to be
loaded to The internal memory of the DSP chip and play it towards Audio output line .
The question is what is the file type of the audio I need to sample that will comply to the
internal digital audio format inside this specific example ?
Is it better to use the SPEECH_ENC_DEC example for that purpose ?
Thanks
Gideon