Hi,
We want to use USB register DEVCTL to check the status of usb cable, but we can not find the address of the DEVCTL in TI documents. Thanks for any help.
Regards,
Yiyuan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We want to use USB register DEVCTL to check the status of usb cable, but we can not find the address of the DEVCTL in TI documents. Thanks for any help.
Regards,
Yiyuan
Hi Patrik,
Thanks for the information. The address 0x8461, which can not be found in TI documents, is actually the one we are using. The problem is the VBUS bits read from 0x8461 do not have consistent results. Do you know the values of AVaid and VBusVaid?
Thanks,
Yiyuan
Hi Yiyuan,
The meanings of bits in DEVCTL are:
_RESV_1 ******** Reserved
BDEVICE 0 - ADEVICE
This Read-only bit indicates whether the USB controller is operating as
the A device or the B device 0: A device 1: B device Only valid
while a session is in progress
FSDEV 0 This Read-only bit is set when a full-speed or high-speed
device has been detected being connected to the port (High-speed
devices are distinguished from full-speed by checking for high-speed
chirps when the device is reset) Only valid in Host mode
LSDEV 0 This Read-only bit is set when a low-speed device has been
detected being connected to the port Only valid in Host mode
VBUS 00 - BELOW These Read-only bits encode the current VBus level
HOSTMODE 0 This Read-only bit is set when the USB controller is acting as a Host
HOSTREQ 0 When set, the USB controller will initiate the Host
Negotiation when Suspend mode is entered. It is cleared when Host
Negotiation is completed. ( B device only)
SESSION 0 When operating as an A device, this bit is set or
cleared by the userto start or end a session When operating as a B
device, this bit is set/cleared by the USB controller when a session
starts/ends It is also set by the user to initiate the Session Request
Protocol. When the USB controller is in Suspend mode, the bit may be
cleared by the user to perform a software disconnect
only information that i have about VBusVaid is:
VBUS 00 - BELOW
These Read-only bits encode the current VBus level as follows ----------------------------------------------
VBus[1] VBus[0] Meaning ------------------------------------------------------------------------------
0 0 Below SessionEnd
0 1 Above SessionEnd, below AValid
1 0 Above AValid, below VBusValid
1 1 Above VBusValid
Hi Patrik,
Thanks.
Do you think we can use 00 - below or other values to make decision on cable connection status, rather using VBusValid (11)?
Thanks,
Yiyuan
Hi Yiyuan,
I think that you should use 11 for VBusValid this is the configuration for "USB Cable Connection Detected".
Regards
Patrik