Part Number: AM625
Tool/software:
I am using am625 Eval board and I was trying understand how to use the (fast) GPI mode of the PRU pins. I was using PRU Header (J10) pins (18, 19 and 20) for testing.
First, I configured the said pins as GPO so I can verify if I can toggle (high/low) in PRU. I used the following settings below and I can confirmed the pins were doing high and low correctly.
AM62X_IOPAD(0x0050, PIN_INPUT, 4) /* (P22) GPMC0_AD5.PR0_PRU0_GPO5 */
AM62X_IOPAD(0x0054, PIN_INPUT, 4) /* (P21) GPMC0_AD6.PR0_PRU0_GPO6 */
AM62X_IOPAD(0x0058, PIN_INPUT, 4) /* (R23) GPMC0_AD7.PR0_PRU0_GPO7 */
Then, I changed the said pins as GPI:
AM62X_IOPAD(0x0050, PIN_INPUT, 5) /* (P22) GPMC0_AD5.PR0_PRU0_GPI5 */
AM62X_IOPAD(0x0054, PIN_INPUT, 5) /* (P21) GPMC0_AD6.PR0_PRU0_GPI6 */
AM62X_IOPAD(0x0058, PIN_INPUT, 5) /* (R23) GPMC0_AD7.PR0_PRU0_GPI7 */
I used this simple pru code:
volatile register uint32_t __R30;
volatile register uint32_t __R31;
#define BIT7 (1 << 7)
#define BIT5 (1 << 5)
void main(void)
{
while (1) {
if (__R31 & BIT7)
Debug_Log("BIT7: High\n\r");
if (__R31 & BIT5)
Debug_Log("BIT5: High\n\r");
}
}
If I assert the pins to high I did not see the change in the input pins. I tried to set