Hi, I've clocked a DM365 at 267 MHz but once Linux (2.6.18 kernel) is running I read /proc/cpuinfo and the "bogomips" field shows 133.5 MHz, is that what's expected? I was expectin 267 bogomips (= same as clock).
I've carefully checked the PLL configuration - using either PLL1 SYSCLK2 or PLL2 SYSCLK2 the "bogomips" are always half of the frequency.
Thanks!
Loic