Tool/software:
I am currently working with the DLP LightCrafter 0.3 WVGA chipset (DLP3000) and am facing an issue with the installation of the Graphical User Interface (GUI). I have downloaded the version of the GUI intended for DLP3010EVM, but the software does not detect the evaluation module (EVM). It shows the status as "Not connected" even though the computer recognizes the USB connection and the DMD screen responds to the connection.
I would appreciate your assistance in one of the following:
- Providing the correct version of the GUI for the DLP3000 chipset.
- Clarifying if the DLP3010EVM GUI is compatible with the DLP3000, and if so, what steps I can take to resolve the connection issue
Best regards,