UIRGENT:
Hello friends,
I have unresolved issues within SYSBIOS project using the SarterWare package in CCSV5.1 using logic PD BSL 4.2.4 on ARM9/OMAPL138 SoM on EVM kit.
I use .gel file supplied by LogicPD for both DSP and ARM9.
First I tested StarterWare "lidd_armv5_omapl138_evmOMAPL138" project and got it working.
Second as a sanity test I created Log example in SYSBIOS and got it working as evident from RTA Raw Logs.
Third I started integrating them.
- I resolved the include errors in beginning by including all those folders that were included in the example "lidd_armv5_omapl138_evmOMAPL138".
- I use the API function definitions of the in the main.c file and created a task to setup, initialise, etc. for LCDC and display a string on it.
- The build gives unresolved symbols for every API calls. I copy some the linker errors here. The full build console output, main.c code, .cfg text is zipped and attached to this thread.
undefined first referenced
symbol in file
--------- ----------------
LIDDAddrIndexSet ./main.obj
LIDDCSTimingConfig ./main.obj
LIDDClkConfig ./main.obj
LIDDDataWrite ./main.obj
LIDDDisplayEnable ./main.obj
LIDDModeSet ./main.obj
LIDDPinMuxSetup ./main.obj
PSCModuleControl ./main.obj
Please tell me what is going wrong in the linking process. I included all the files it seems or any thing missing?
File :6765.a2.txt
Please reply soon.
With warm regards.
Mahesh