Part Number: AM625
Tool/software:
Hello TI,
Could you suggest how to fix below weston touch issue?
oot@am62xx-evm:~# weston &
---log--
18:34:49.658] GL ES 3.1 - renderer features:
read-back format: BGRA
wl_shm sub-image to texture: yes
EGL Wayland extension: yes
[18:34:49.659] couldn't fstat launcher tty: Bad file descriptor
[18:34:49.835] event0 - goodix-ts: is tagged by udev as: Tablet
[18:34:49.836] event0 - goodix-ts: libinput bug: missing tablet capabilities: resolution. Ignoring this device.
[18:34:49.836] event0 - goodix-ts: device is a tablet
[18:34:49.869] event0 - failed to create input device '/dev/input/event0'
----------
On Weston GUI, there is no response when we touch (but touch sensor works fine).
This issue is same as below:
Log: