Tool/software:
Hi Krunal & TI team,
Good Day!
As informed to Krunal & TI team in email communications, we would like to use the Quad SPI Serial Nand Flash interface with a density of 2G-bit (i.e. 256MB) in-order to work with AM62x MPU.
However as it was informed by Krunal(TI) - " AM62x ROM do not support “QE Mode” and also already one of TI’s other customer ran into an “issue with QE bit” . "
Hence, we request TI's support on the below in-order that we don’t run into any such known technical issues..
- Can you please let us the suitable part number of QSPI Nand flash with a memory density of 2G-bit (i.e. 256MB) which is supported by AM62x MPU ?
- For better clarity, can you please help in filling the below table to understand the support & validation of AM62x MPU with QSPI Nand Flash part numbers ?
This will really enable us to select the Correct QSPI Nand flash part number which is supported by AM62x MPU.
|
SL No |
Manufacturer Part Number |
Part Description |
Supported by TI AM62x |
Validated by TI using AM62x EVM |
TI's Design Recommendation to use with AM62x MPU |
TI's Remarks |
|
1 |
W35N01JWTBAG |
1G-bit, Octal NAND Flash memory, 1.7V to 1.95V, |
Yes / No ? |
Yes / No ? |
Yes / No ? |
Tested on TI EVM with modifications |
|
2 |
W25N01JWTBAG |
1G-bit, DUAL/QUAD SPI NAND Flash memory, 1.7V to 1.95V, |
Yes / No ? |
Yes / No ? |
Yes / No ? |
Tested on TI EVM with modifications |
|
3 |
W25N02KWxxxx |
2G-bit Serial SLC NAND Memory, 1.7V to 1.95V |
Yes / No ? |
Yes / No ? |
Yes / No ? |
It was tested by TI's other customer. |
|
4 |
W25N02KWZEIR |
2G-bit Serial SLC NAND Memory, 1.7V to 1.95V, |
Yes / No ? |
Yes / No ? |
Yes / No ? |
|
|
5 |
W25N02KWTBIR |
2G-bit Serial SLC NAND Memory, 1.7V to 1.95V, |
Yes / No ? |
Yes / No ? |
Yes / No ? |
|
|
6 |
W25N02JWZEIC |
2G-bit DUAL/QUAD SPI SLC NAND Memory, 1.7V to 1.95V, |
Yes / No ? |
Yes / No ? |
Yes / No ? |
|
|
7 |
W25N02JWTBIC |
2G-bit DUAL/QUAD SPI SLC NAND Memory, 1.7V to 1.95V, |
Yes / No ? |
Yes / No ? |
Yes / No ? |
|
|
8 |
W35N02JWTBIF |
2G-bit, Octal NAND Flash memory, 1.7V to 1.95V, |
Yes / No ? |
Yes / No ? |
Yes / No ? |
|