Hello
I want to run I2S protocol on the McBSP. The DSP is configured as slave and receives a bit clock and frame select. The audio format is 16 bit for left and right channel.
Question 1:
How do the McBSP react when the word select is high for 16 bit clock cycles? Does the McBSP resync for every bit clock when word select is high? I don’t find any information about that in the Technical Reference Manual. Or do I have to activate ignore (RFIG/XFIG?
Question 2:
How do I synchronize the transmitting and receiving so that the samples for left and right end up correctly? I could end up so the left and right channels are swapped.