AM62A3: Unable to transmit and receive data on CAN Bus

Part Number: AM62A3

Tool/software:

Hello TI,
    We are trying to integrate MCAN on AM62A3 Evalution board. But getting the bellow observations : 

root@am62axx-evm:~# candump main_mcan0
[   69.474298] can: controller area network core
[   69.474370] NET: Registered PF_CAN protocol family
[   69.480188] can: raw protocol

We have added the k3-am62x-sk-mcan.dtbo file in the u-boot setenv as suggested in Topic- 9.1.6.6 in the below link for 09.02 build version : 

https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_02_01_10/exports/docs/linux/How_to_Guides/Target/How_to_test_MCAN_on_AM62x.html#testing-1x-mcan-on-am62x-and-1x-mcan-on-am64x

But unable to get any data on candump, nor able to send data through cansend command. We have connected the CAN_TX pin to the TX pin of the Transciever and CAN_RX pin to the RX pin of the transciever. The HIGH and LOW pins on the transciever is conneted to the CAN device that is transmitting data at 1Mbps. 


Please, let us know what else we are missing.