This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8147 to drive a 24b (RGB888), TFT, LCD display. Is a direct connection possible?



From custoer: I am looking for info on how the DM8147 can be connected to drive a 24b (RGB888), TFT, LCD display. Is a direct connection possible?

  • Adam,

    This is a bit of a vague question to be honest, and depends really on the particular LCD panel in question.

    If the LCD panel accepts CMOS level parallel inputs, then yes. If the panel is a higher resolution that uses LVDS signalling then an LVDS serializer is needed.

    Have a look at the following Wiki page for some additional information. This Wiki was originally written for OMAP3, but is very much appropriate to the DM81xx devices.

    http://processors.wiki.ti.com/index.php/LCD_connectivity

    BR,

    Steve