TDA4VE-Q1: TDA4 to run run_app_tidl.sh is Failed ?

Part Number: TDA4VE-Q1

Tool/software:

Hi 

I have a TDA4 J721s2-evm

I Want to run the DEMO

./run_app_tidl.sh                     - Image classification demo (needs display)

But I can not run the "run_app_tidl.sh"

it appears this message

root@j721s2-evm:/opt/vision_apps# ./run_app_tidl.sh
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=5) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
93.704896 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
93.707200 s: VX_ZONE_INIT:Enabled
93.707231 s: VX_ZONE_ERROR:Enabled
93.707238 s: VX_ZONE_WARNING:Enabled
93.709898 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
93.712014 s: VX_ZONE_INIT:[tivxHostInitLocal:101] Initialization Done for HOST !!!
app_tidl: ERROR: Unable to open IO config file /opt/vision_apps/test_data/tivx/tidl_models/tidl_io_mobilenet_v1_1.bin
app_tidl: ERROR: Unable to open network file /opt/vision_apps/test_data/tivx/tidl_models/tidl_net_mobilenet_v1.bin
93.720068 s: VX_ZONE_ERROR:[tivxAddKernelTIDL:269] invalid values for num_input_tensors or num_output_tensors
93.734001 s: VX_ZONE_ERROR:[tivx_utils_bmp_read:867] Failed to open file </opt/vision_apps/test_data/tivx/tidl_models/ti_logo.bmp>.
93.742057 s: VX_ZONE_ERROR:[vxQueryKernel:140] Invalid kernel reference
93.742085 s: VX_ZONE_ERROR:[vxMapUserDataObject:384] Invalid user data object reference
93.742094 s: VX_ZONE_ERROR:[vxUnmapUserDataObject:469] Invalid user data object reference
93.742120 s: VX_ZONE_ERROR:[vxCreateNodeByStructure:91] failed to retrieve kernel enum 0
93.744979 s: VX_ZONE_ERROR:[vxSetReferenceName:960] Invalid reference
93.744994 s: VX_ZONE_ERROR:[vxSetReferenceName:960] Invalid reference
93.745003 s: VX_ZONE_ERROR:[vxSetReferenceName:960] Invalid reference
93.745009 s: VX_ZONE_ERROR:[vxSetReferenceName:960] Invalid reference
93.746551 s: VX_ZONE_ERROR:[ownContextSendCmd:822] Command ack message returned failure cmd_status: -1
93.746569 s: VX_ZONE_ERROR:[ownContextSendCmd:862] tivxEventWait() failed.
93.746577 s: VX_ZONE_ERROR:[ownNodeKernelInit:584] Target kernel, TIVX_CMD_NODE_CREATE failed for node DisplayNode
93.746583 s: VX_ZONE_ERROR:[ownNodeKernelInit:585] Please be sure the target callbacks have been registered for this core
93.746590 s: VX_ZONE_ERROR:[ownNodeKernelInit:586] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
93.746598 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.display ... failed !!!
93.746613 s: VX_ZONE_ERROR:[vxVerifyGraph:2059] Node kernel init failed
93.746621 s: VX_ZONE_ERROR:[vxVerifyGraph:2113] Graph verify failed
app_tidl: ERROR: Verifying display graph ... Failed !!!
93.746711 s: VX_ZONE_ERROR:[ownReleaseReferenceInt:601] Invalid reference
93.746725 s: VX_ZONE_ERROR:[ownReleaseReferenceInt:601] Invalid reference
93.746732 s: VX_ZONE_ERROR:[ownReleaseReferenceInt:601] Invalid reference
93.747424 s: VX_ZONE_ERROR:[vxRemoveKernel:287] Invalid kernel reference
93.750213 s: VX_ZONE_INIT:[tivxHostDeInitLocal:115] De-Initialization Done for HOST !!!
[MCU2_0] 93.746288 s: src/drv/disp/dss_dispApi.c @ Line 336:
[MCU2_0] 93.746316 s: Display Controller registration failed for DSS
[MCU2_0] 93.746359 s: VX_ZONE_ERROR:[tivxDisplayCreate:547] DISPLAY: ERROR: Display Create Failed!
93.752738 s: VX_ZONE_INIT:[tivxDeInitLocal:193] De-Initialization Done !!!
APP: Deinit ... !!!
REMOTE_SERVICE: Deinit ... !!!
REMOTE_SERVICE: Deinit ... Done !!!
IPC: Deinit ... !!!
IPC: DeInit ... Done !!!
MEM: Deinit ... !!!
DDR_SHARED_MEM: Alloc's: 9 alloc's of 20104316 bytes
DDR_SHARED_MEM: Free's : 9 free's of 20104316 bytes
DDR_SHARED_MEM: Open's : 0 allocs of 0 bytes
MEM: Deinit ... Done !!!
APP: Deinit ... Done !!!

Please tell me which step I did wrong?

thanks