Hi -
We are trying to use the PinMux Utility, v2.2.0, to pin out our DM8148 device.
We require the use of both EMAC0 as RMII and EMAC1 as RGMII.
I don't seem to be able to get to the EMAC1 pins (as defined in Table 3-7 of SPRS647B - March 2011– Revised Sept 2011- TMS320DM814x datasheet) for RGMII when I select EMAC1 in the PinMux Peripheral Interfaces block. The pins are tied up in the Fcn1 Column of the EMAC(0) PinMux Peripheral Interfaces block.
I was under the impression that I could use both EMAC0 and EMAC1 in these modes.
Is there some pin use rule I am breaking? I've defined several interfaces, approx. 50 balls, with no conflicts, all green.
Also, is there a way to export the info in the Pin Mux Grid directly to a spreadsheet?
Thanks -
Sal