Other Parts Discussed in Thread: AM3517
Another discussion that will hopefully save someone else some time.
The linux-devkit toolchain in the version 05.02.00.00 SDK has a problem with missing definitions for AF_CAN and PF_CAN.
I'm starting to work with the CAN interface on my am3517 EVM, and trying to use the socketCAN interface to communicate with it.
Building a simple test program to open a socketCAN socket and bind to it, compilation failed due to missing these definitions.
I am building in code composer studio and can see in the includes section in project explorer under my project, all the include paths are in linux-devkit.
find . -name socket.h turns up all of these, which I then grep to see which have socket family definitions:
grep AF_INET usr/include/netlink/socket.h
grep AF_INET usr/include/sys/socket.h
grep AF_INET usr/include/linux/socket.h
grep AF_INET usr/include/bits/socket.h
grep AF_INET usr/include/asm-generic/socket.h
grep AF_INET usr/include/asm/socket.h
only 2 have AF_INET definitions, do they have AF_CAN?
grep AF_CAN usr/include/linux/socket.h
grep AF_CAN usr/include/bits/socket.h
My project includes linux/socket.h but some tricky ifdef'ing apparently prevents it from defining those constants.
And bits/socket.h is missing them. So it had to be the culprit.
I added the definitions there, and the build worked.