This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM68: SK AM68 Function Related Questions

Part Number: SK-AM68
Other Parts Discussed in Thread: AM68A, AM68, AM69, AM67A

Tool/software:

Subject: Inquiry Regarding SK-AM68 Starter Kit Features

Hello, 

I have a few questions regarding the SK-AM68 before making a purchase.

1. The SK-AM68 is listed as having an 8 TOPS NPU in its features, but I could not find this information in the User Guide. I would like to confirm if there is a separate Starter Kit that includes the AM68a SoC.

2. Does the board support 12-bit RGB-IR input? Additionally, I noticed that the board provides 480 MPixel/s ISP. Can the ISP be tuned to match the specifications of the camera we have selected? If so, could you also provide the tuning cost per camera channel?

3. Lastly, I would appreciate it if you could share details regarding the NRE (Non-Recurring Engineering) cost and software license fees.

Thank you, and I look forward to your response.

Best regards,
[jaehwan shin]

  • Hi jaehwan,...

    I would like to confirm if there is a separate Starter Kit that includes the AM68a SoC.

    https://www.ti.com/tool/SK-AM68#tech-docs

    There seems only one common SK-AM68 board according to the page above.

    2. Does the board support 12-bit RGB-IR input? Additionally, I noticed that the board provides 480 MPixel/s ISP. Can the ISP be tuned to match the specifications of the camera we have selected? If so, could you also provide the tuning cost per camera channel?

    If you are looking for 12-bit RGB-IR 4x4 raw image sensor support by ISP (VPAC), AM68/AM69 ISP (VPAC3) are not able to do that.

    Only, AM62A and AM67A (with VPAC3L) can support 4x4 raw images (e.g., https://www.ti.com/tool/J722SXH01EVM).

    3. Lastly, I would appreciate it if you could share details regarding the NRE (Non-Recurring Engineering) cost and software license fees.

    I am not aware of any of these are required for TI TDA4/AM6xA SDK.