Other Parts Discussed in Thread: AM62A7
Tool/software:
Hello TI experts,
We met issue that we can't preview 4 cameras about 3M resolution (1920x1536) in the same time but 3 cameras about 3M resolution (1920x1536) in the same time can.
We also tried single previewing each camera about 3M resolution (1920x1536) with proper matching virtual channel (powered on and initialized one by one), and all of them are works.
How could we check the MIPI CSI2 status and adjust setting to make 4 cameras about 3M resolution (1920x1536) previewing in the same time working?
We already adjusted reserved C7 shared memory from 288MB to be 864MB, MIPI RX Clock 1.1 GHz and 4 lanes about MIPI CSI2 Data.
The enable_streams of v4l2_subdev_pad_ops called and working with g-streamer pipe setting but the video is not showing.
Customized board with AM62A7-Q1
TI SDK BSP version: V09_00_02
Linux version: 6.1.80
Total needed data: 3M x RAW10 x 30fps x 4 ports = 3.6 Gbps
Data loading per Lane : 900 Mbps
Needed data loading per Camera: 900 Mbps