This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: Reduce the rate of mmc0

Part Number: AM623

Tool/software:

Hi, TI expert! 

I have a development environment for am6234, with our own evaluation board.

The software SDK version is PROCESSOR-SDK-LINUX-RT-AM62X-08.06.00.42.

The current mmc0 speed of our board is hs200, as shown below:


The corresponding device tree configuration is as follows:

	sdhci0: mmc@fa10000 {
		compatible = "ti,am62-sdhci";
		reg = <0x00 0xfa10000 0x00 0x260>, <0x00 0xfa18000 0x00 0x134>;
		interrupts = <GIC_SPI 133 IRQ_TYPE_LEVEL_HIGH>;
		power-domains = <&k3_pds 57 TI_SCI_PD_EXCLUSIVE>;
		clocks = <&k3_clks 57 5>, <&k3_clks 57 6>;
		clock-names = "clk_ahb", "clk_xin";
		assigned-clocks = <&k3_clks 57 6>;
		assigned-clock-parents = <&k3_clks 57 8>;
		mmc-ddr-1_8v;
		mmc-hs200-1_8v;
		ti,trm-icp = <0x2>;
		bus-width = <8>;
		ti,clkbuf-sel = <0x7>;
		ti,otap-del-sel-legacy = <0x0>;
		ti,otap-del-sel-mmc-hs = <0x0>;
		ti,otap-del-sel-ddr52 = <0x5>;
		ti,otap-del-sel-hs200 = <0x5>;
		ti,itap-del-sel-legacy = <0xa>;
		ti,itap-del-sel-mmc-hs = <0x1>;
		status = "okay";
	};
	

&main_pmx0 {
        main_mmc0_pins_default: main-mmc0-pins-default {
                pinctrl-single,pins = <
                        AM62X_IOPAD(0x220, PIN_INPUT, 0) /* (Y3) MMC0_CMD */
                        AM62X_IOPAD(0x218, PIN_INPUT, 0) /* (AB1) MMC0_CLK */
                        AM62X_IOPAD(0x214, PIN_INPUT, 0) /* (AA2) MMC0_DAT0 */
                        AM62X_IOPAD(0x210, PIN_INPUT, 0) /* (AA1) MMC0_DAT1 */
                        AM62X_IOPAD(0x20c, PIN_INPUT, 0) /* (AA3) MMC0_DAT2 */
                        AM62X_IOPAD(0x208, PIN_INPUT, 0) /* (Y4) MMC0_DAT3 */
                        AM62X_IOPAD(0x204, PIN_INPUT, 0) /* (AB2) MMC0_DAT4 */
                        AM62X_IOPAD(0x200, PIN_INPUT, 0) /* (AC1) MMC0_DAT5 */
                        AM62X_IOPAD(0x1fc, PIN_INPUT, 0) /* (AD2) MMC0_DAT6 */
                        AM62X_IOPAD(0x1f8, PIN_INPUT, 0) /* (AC2) MMC0_DAT7 */
                >;
        };
};

&sdhci0 {
        pinctrl-names = "default";
        pinctrl-0 = <&main_mmc0_pins_default>;
        ti,driver-strength-ohm = <50>;
        non-removable;
        disable-wp;
};

If I want to reduce the speed of mmc0, such as from hs200 to sdr104, how do I modify the device tree?

Regards,

Li

  • Hello,

    If I want to reduce the speed of mmc0, such as from hs200 to sdr104, how do I modify the device tree

    For configuring the mmc to certain speed mode X, you should comment the "ti,otap-del-sel-*" properties of all higher speed modes than X.

    For example, the following patch initializes the mmc in ddr52 spped mode.

    diff --git a/arch/arm64/boot/dts/ti/k3-am62-main.dtsi b/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
    index 510775e9a88f..e7c33d913962 100644
    --- a/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
    +++ b/arch/arm64/boot/dts/ti/k3-am62-main.dtsi
    @@ -509,7 +509,7 @@ sdhci0: mmc@fa10000 {
     		ti,otap-del-sel-legacy = <0x0>;
     		ti,otap-del-sel-mmc-hs = <0x0>;
     		ti,otap-del-sel-ddr52 = <0x5>;
    -		ti,otap-del-sel-hs200 = <0x5>;
    +		// ti,otap-del-sel-hs200 = <0x5>;
     		ti,itap-del-sel-legacy = <0xa>;
     		ti,itap-del-sel-mmc-hs = <0x1>;
     	};
    

    Regards,

    Prashant