Other Parts Discussed in Thread: TVP7002
Hi,
I want to run the Capture_Encode examples in ezsdk_5_02 . And my filesystem is ezsdk-dm816x-evm-rootfs.tar.gz available in
filesystem directory. Because I don't have HD 1080p 60 video source which is in RGB formate for J7-J6-J5 connectors, can i use other
video input connectors (eg. HDMI connector ) to run this demo? If can how to connect the evm board with the video source?
By now I have connected 1080p_60 component input to EIO card's first TVP7002 chip (J7-J6-J5 connectors are Y/Pb/pr), components
go to executing state but I don't see video output on Onchip HDMI connector of EVM board. Cann't J7-J6-J5 connectors receive
Y/Pb/pr video signal ?
Thanks in advance,
xavier