This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM67: How to configure DTS of RS485 to enable flow control?

Part Number: AM67
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hi 

Customer are implementing HW flow control based on AM67.

Here they use UART1 UART2 UART3 UART4 UART5 UART6.

For UART1 and UART2, they use UART_RTS pin. For other UART, they use general GPIO.

UART1-UART2

UART3 - UART6

And here is their DTS file, could you help check three things?

k3-j722s-ecu1270.dts

1. If need implement flow control, UART_RTS pin is necessary for rts-GPIO? Can general GPIO be used as rts-GPIO for UART3 - UART6?

2. For UART1 and UART2, the DTS configuration is right or not?

3. Is SW flow control in SDK ready or just HW flow control?

Regards

Zekun