This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Single DEI output

Hi

 

DM8168 EVM using ezsdk 5.02.01.59

I want to Use the DEI but do not want to display, I only want to send  data to Encoder. Is this possible??

Back ground:

I would like to convert a stream of HDMI DATA(HDMI camera sreaming into FPGA and into bufffer which is consumed by the DEI)  and encode it to a H.264 stream.

As a test to just get the DEI working with the Encoder. I have setup 2 components  OMX.TI.VPSSM3.VFPC.DEIHDUALOUT  and  OMX.TI.DUCATI.VIDENC.  (I setup  buffers which I populate with a colour bar and pass it to the DEI whcih outputs to the ENC. My  set up with call backs works because the Parameters are set when I call OMX_GetHandle. First I setup the DEI Handle This returns OK  Enabling the Output ports first which only works if I enable OMX_VFPC_OUTPUT_PORT_START_INDEX this works fine  (I presume this is port 16)

( next ) if I enable OMX_VFPC_OUTPUT_PORT_START_INDEX + 1 my program stops at the SempPend and freezes.

I then Enable Input port OMX_VFPC_INPUT_PORT_START_INDEX  = 0 this works fine if I ommit the last line.

I then setup the encoder input and output port (fine)

When i Allocate buffers the DEI  allocates buffers for the DEI Output and Input for that  component and then freezes at SempPend

So my questions are .

Question 1

Can I set the DEI to use a single output port or do I have to configure 2 output ports ?

Question 2

Why does the code stop when I try enable the second output port (If I leave this out and only enable the input and output it carrys on)?

Question 3

Why does my code stop at SempPend when I set up the ALLOCATE buffer comand on the input and output buffers (I alocate all input buffers and then all output buffers and then pend on Semaphore)?

Question 4

Do I have to setup the DEI number of inputs and ou puts and start index's using the "OMX_IndexParamVideoInit" command ?

Question 5

Can I fill a buffer with grey and give it to the DEI like the VPCC would?

 

Thanks

Robin

static OMX_ERRORTYPE VidEncSetDeiParams (OMX_PTR ptrAppData)
{   //TODO
 TVidComponent *pComp;
 pComp = ptrAppData;
 TVidDeiParams* pParams = (TVidDeiParams*) pComp->pParams;
 OMX_ERRORTYPE eError = OMX_ErrorNone;
 OMX_PARAM_BUFFER_MEMORYTYPE memTypeCfg;
 OMX_PARAM_PORTDEFINITIONTYPE paramPort;
 OMX_PARAM_VFPC_NUMCHANNELPERHANDLE sNumChPerHandle;
 //OMX_CONFIG_ALG_ENABLE algEnable;
 OMX_CONFIG_VIDCHANNEL_RESOLUTION chResolution;
// OMX_PORT_PARAM_TYPE portInit;

 

 /* Setting Memory type at input port to Raw Memory */
 OMX_INIT_PARAM (&memTypeCfg);
 memTypeCfg.nPortIndex = pComp->nPortInput;
 memTypeCfg.eBufMemoryType = OMX_BUFFER_MEMORY_DEFAULT;
 eError = OMX_SetParameter (pComp->pHandle, OMX_TI_IndexParamBuffMemType,
   &memTypeCfg);
 if (eError != OMX_ErrorNone)
 {
  printf ("failed to set memory Type at input port\n");
 }

 /* Setting Memory type at output port 16 to Raw Memory */
 OMX_INIT_PARAM (&memTypeCfg);
 memTypeCfg.nPortIndex = pComp->nPortOutput;
 memTypeCfg.eBufMemoryType = OMX_BUFFER_MEMORY_DEFAULT;
 eError = OMX_SetParameter (pComp->pHandle, OMX_TI_IndexParamBuffMemType,
   &memTypeCfg);
 if (eError != OMX_ErrorNone)
 {
  printf ("failed to set memory Type at output port\n");
 }

// /* Setting Memory type at output port 17  to Raw Memory */
//  OMX_INIT_PARAM (&memTypeCfg);
//  memTypeCfg.nPortIndex = pComp->nPortOutput + 1;
//  memTypeCfg.eBufMemoryType = OMX_BUFFER_MEMORY_DEFAULT;
//  eError = OMX_SetParameter (pComp->pHandle, OMX_TI_IndexParamBuffMemType,
//    &memTypeCfg);
//  if (eError != OMX_ErrorNone)
//  {
//   printf ("failed to set memory Type at output port\n");
//  }


 /* set input height/width and colour format input port */
 OMX_INIT_PARAM (&paramPort);
 paramPort.nPortIndex = pComp->nPortInput;
    OMX_GetParameter (pComp->pHandle, OMX_IndexParamPortDefinition, &paramPort);
 paramPort.nPortIndex = pComp->nPortInput;
 paramPort.eDir = OMX_DirInput;
 paramPort.format.video.nFrameWidth = pParams->nWidth;
 paramPort.format.video.nFrameHeight = pParams->nHeight;
 paramPort.format.video.nStride = pParams->nWidth;
 paramPort.format.video.eCompressionFormat = OMX_VIDEO_CodingUnused;
 paramPort.format.video.eColorFormat = OMX_COLOR_FormatYUV420SemiPlanar;
    paramPort.nBufferSize =(paramPort.format.video.nStride * pParams->nHeight * 3) >> 1;
    /*set buffer size to allocate buffers*/
    pComp->nInPortBufferSize = paramPort.nBufferSize;
 paramPort.nBufferAlignment = 0;
 paramPort.bBuffersContiguous = 0;
 paramPort.nBufferCountActual = pComp->nInputBuffers;
 printf ("set input port params (width = %u, height = %u) \n",(int)pParams->nWidth, (int)pParams->nHeight);
 OMX_SetParameter (pComp->pHandle, OMX_IndexParamPortDefinition, &paramPort);

 /*set output height/width and colour format Output port 16 */
 OMX_INIT_PARAM (&paramPort);
 paramPort.nPortIndex = pComp->nPortOutput;
 OMX_GetParameter (pComp->pHandle, OMX_IndexParamPortDefinition,&paramPort);
 paramPort.nPortIndex = OMX_VFPC_OUTPUT_PORT_START_INDEX;
 paramPort.eDir = OMX_DirOutput;
 paramPort.format.video.nFrameWidth = pParams->nWidth;
 paramPort.format.video.nFrameHeight = pParams->nHeight;
 paramPort.format.video.eCompressionFormat = OMX_VIDEO_CodingUnused;
 paramPort.nBufferAlignment = 0;
 //paramPort.nBufferCountActual = pComp->nOutputBuffers/2;
 paramPort.nBufferCountActual = pComp->nOutputBuffers;
 paramPort.format.video.nStride = pParams->nWidth;
 /* This port is connected to encoder and provides 420 o/p */
 paramPort.nBufferSize = (paramPort.format.video.nStride * paramPort.format.video.nFrameHeight * 3) >> 1;
 pComp->nOutPortBufferSize = paramPort.nBufferSize;
 printf ("set output port 1 params (width = %d, height = %d )\n",(int) pParams->nWidth,(int)pParams->nHeight);
 OMX_SetParameter (pComp->pHandle, OMX_IndexParamPortDefinition, &paramPort);

 

 

 

 OMX_INIT_PARAM (&sNumChPerHandle);
 sNumChPerHandle.nNumChannelsPerHandle = 1;
 eError = OMX_SetParameter (pComp->pHandle, (OMX_INDEXTYPE) OMX_TI_IndexParamVFPCNumChPerHandle, &sNumChPerHandle);
 printf ("set number of channels %d \n",(int)sNumChPerHandle.nNumChannelsPerHandle);
 if (eError != OMX_ErrorNone)
 {
  printf ("failed to set num of channels\n");
 }

 /* set VFPC input and output resolution information */
 printf ("set input resolution\n");

 OMX_INIT_PARAM (&chResolution);
 chResolution.Frm0Width = pParams->nWidth;
 chResolution.Frm0Height = pParams->nHeight;
 chResolution.Frm0Pitch = pParams->nWidth;;
 chResolution.Frm1Width = 0;
 chResolution.Frm1Height = 0;
 chResolution.Frm1Pitch = 0;
 chResolution.FrmStartX = 0;
 chResolution.FrmStartY = 0;
 chResolution.FrmCropWidth = pParams->nWidth;
 chResolution.FrmCropHeight = pParams->nHeight;
 chResolution.eDir = OMX_DirInput;
 chResolution.nChId = 0;

 eError = OMX_SetConfig (pComp->pHandle,
   (OMX_INDEXTYPE) OMX_TI_IndexConfigVidChResolution,
   &chResolution);
 if (eError != OMX_ErrorNone)
 {
  printf ("failed to set input channel resolution\n");
 }

 printf ("set output resolution\n");
 OMX_INIT_PARAM (&chResolution);
 /* first output to display */
 chResolution.Frm0Width = pParams->nWidth;
 chResolution.Frm0Height = pParams->nHeight;
 chResolution.Frm0Pitch = pParams->nWidth;
 /* second output to encode */
 chResolution.Frm1Width = pParams->nWidth;
 chResolution.Frm1Height = pParams->nHeight;
 chResolution.Frm1Pitch = pParams->nWidth;
 chResolution.FrmStartX = 0;
 chResolution.FrmStartY = 0;
 chResolution.FrmCropWidth = 0;
 chResolution.FrmCropHeight = 0;
 chResolution.eDir = OMX_DirOutput;
 chResolution.nChId = 0;

 eError = OMX_SetConfig (pComp->pHandle,
   (OMX_INDEXTYPE) OMX_TI_IndexConfigVidChResolution,
   &chResolution);
 if (eError != OMX_ErrorNone)
 {
  printf ("failed to set output channel resolution\n");
 }

return eError

}