Other Parts Discussed in Thread: WL1837MOD, AM625
Tool/software:
We have made a custom board based on the SK-AM62 (we have changed the soc to AM6231ASGGGAALW but are using the same RAM as reference board)and trying to boot a yocto based image onto the board. We first tested the image on the SK-AM62 and it works as intended but when we try and boot the same image on our board we are facing issues. We are booting over the SD card (MMC1) (we have removed the sd card connector and brought the signal onto a header and using Pmod MicroSD adapter to interface the card) and the U-boot is loading but we are not getting any further. We tried the default minimal image provided by TI and even that produced the same results. We are getting the following output on console.
When we enable debug we are getting the following output. We connected the sd card to MMC2 as it was showing in the log that it was "Trying to boot from MMC2" on console. We have removed the "WL1837MOD" Wi-Fi/Bluetooth module and brought the signals to a header so we used the Pmod MicroSD adapter to connect the sd card, but we didn't get any output on the console as well as the current draw remained same as it was without boot media.
Could you help identify the reason for not receiving any additional logs and assist us with the bring-up process?