Other Parts Discussed in Thread: SYSBIOS
Hello,
I'm using SYSBIOS v6.31.04.37 including NDK v2.20.0.19 on a OMAPL138Evm board. Depending on our application I have to write a SYSBIOS program which loads AIS-files and start other SYSBIOS applications via Ethernet (TFTP). These applications are completely independent projects including c_init, sysbios,ndk,etc.
My first idea was to write a sysbios-program which loads a chosen AIS-file into memory, stops the ndk-stack by NC_Stop, stops the SYSBIOS by BIOS_exit and jump to the c_init vector of the loaded application. The problem is that the BIOS_exit function never returns and ends in a loader_exit function.
Exists any way for a controlled shutdown of ndk and SYSBIOS with having the oportunity to jump to a new application code?
Best regards,
Klaus Peter