Part Number: AM62A7
Tool/software:
Hello,team
Environment: AM62A7 SDK 09_02_00_05
We occasionally encounter the following error during startup. What is the reason for this problem?
SYSFW Firmware Version 9.2.7--v09.02.07 (Kool Koala) SYSFW Firmware revision 0x9 SYSFW ABI revision 3.1 stage 2 program flag : 000000000000 stage2 appImageOffset = 0xC0000. [BOOTLOADER_PROFILE] Boot Media : eMMC [BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz [BOOTLOADER_PROFILE] Boot Image Size : 6415 KB [BOOTLOADER_PROFILE] Cores present : hsm-m4f0-0 r5f0-0 a530-0 c75ss0 [BOOTLOADER PROFILE] System_init : 1931us [BOOTLOADER PROFILE] Board_init : 0us [BOOTLOADER PROFILE] Drivers_open : 21757us [BOOTLOADER PROFILE] Board_driversOpen : 0us [BOOTLOADER PROFILE] Sciclient Get Version : 10290us [BOOTLOADER PROFILE] App_loadImag Received: es : 10162us [BOOTLOADER PROFILE] App_loadSelfcoreImage : 15127us [BOOTLOADER PROFILE] App_loadLinuxImages : 23417us [BOOTLOADER PROFILE] App_loadDSPImages : 140251us [BOOTLOADER_PROFILE] SBL Total Time Taken : 222940us Image loading done, switching to application ... Starting linux and RTOS/Baremetal applications NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 ERROR: Timeout waiting for thread SP_RESPONSE to fill ERROR: Thread SP_RESPONSE verification failed (-60) ERROR: Message receive failed (-60) ERROR: Failed to get response (-60) ERROR: Transfer send failed (-60) ERROR: Timeout waiting for thread SP_RESPONSE to fill ERROR: Thread SP_RESPONSE verification failed (-60) ERROR: Message receive failed (-60) ERROR: Failed to get response (-60) ERROR: Transfer send failed (-60) ERROR: Unable to query firmware capab Received: ilities (-60) E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 ti_sci_init:486 Unable to communicate with control firmware (-65523) E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x0006fae0 failed E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) Received: E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 tee_otp_get_hw_unique_key:97 Could not get HUK E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x0006fb08 failed Received: E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523 E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523) E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523) E/TC:0 0 sa2ul_init:106 Could not change TRNG firewall owner E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x0006fb10 failed E/TC:0 0 E/TC:0 0 Core data-abort at address 0x14 (translation fault) E/TC:0 0 esr 0x96000005 ttbr0 0x9e8a1000 ttbr1 0x00000000 cidr 0x0 E/TC:0 0 cpu #0 cpsr 0x600003c4 E/TC:0 0 x0 000000009e874000 x1 0000000000000000 E/TC:0 0 x2 0000000000000000 x3 0000000000000000 E/TC:0 0 x4 00000000000003a0 x5 Received: 000000009e891d70 E/TC:0 0 x6 ffffffffffffffb0 x7 0000000000010cb0 E/TC:0 0 x8 000000009e891f80 x9 000000009e881070 E/TC:0 0 x10 0000000000000042 x11 0000000000000008 E/TC:0 0 x12 0000000000000000 x13 000000009e8a9050 E/TC:0 0 x14 0000000000000000 x15 0000000000000000 E/TC:0 0 x16 000000009e81c67c x17 0000000000000000 E/TC:0 0 x18 0000000000000000 x19 000000009e8a93d0 E/TC:0 0 x20 000000009e8a93d8 x21 000000009e874000 E/TC:0 0 x22 000000009e874000 x23 000000009e874ee0 E/TC:0 0 x24 000000009e873db0 x25 0000000000000000 E/TC:0 0 x26 0000000000000000 x27 0000000000000000 E/TC:0 0 x28 0000000000000000 x29 000000009e8a9360 E/TC:0 0 x30 000000009e816fcc elr 000000009e816fdc E/TC:0 0 sp_el0 000000009e8a9360 E/TC:0 0 TEE load address @ 0x9e800000 E/TC:0 0 Call stack: E/TC:0 0 0x9e816fdc E/TC:0 0 0x9e807d24 E/TC:0 0 0x9e822148 E/TC:0 0 0x9e807e94 E/TC:0 0 Panic 'unhandled pageable abort' at core/arch/arm/kernel/abort.c:582 <abort_handler> E/TC:0 0 TEE load address @ 0x9e8000 Received: 00 E/TC:0 0 Call stack: E/TC:0 0 0x9e80801c E/TC:0 0 0x9e81eb88 E/TC:0 0 0x9e807920 E/TC:0 0 0x9e804a98
Best regards,
XUE Fadong