Part Number: AM6442
Tool/software:
Folks:
After downloading the MCU plus & Linux SDK ver 10.1
I saw some discrepancies & concerns on these URLs
- https://software-dl.ti.com/mcu-plus-sdk/esd/AM64X/10_01_00_32/exports/docs/build_sheet/am64x-sw-buildsheet.html
- https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/10_01_10_04/exports/docs/devices/AM64X/AM64X_build_sheet_10_01_10_04_files/AM64X_build_sheet_10_01_10_04.htm
(should they should have identical content?)
By Category > Module > SubModule
Processors and Accelerators >
Dual-R5F MCU Subsystem -- should that be listed as a Quad - or are you accounting for 2 Dual-R5F subsystems?
Dual-A53 MPU subsystem - wrt RTOS on A53 -- as long as you do not insinuate that one could SMP between the Dual-A53 in FreeRTOS - but in the MCU+ release notes you say that A53 FreeRTOS is experimental - that is inconsistency.
"Programmable Real-Time Unit and Industrial Communication Subsystem - Gigabit" - that cell needs a word-wrap of text
High-speed Serial Interfaces >
Universal Serial Bus Subsystem (USBSS) > Device 3.0 - big error (confirm with Bin Lu) - Linux on A53 is a NO.
Industrial and Control Interfaces>
Enhanced Quadrature Encoder Pulse (EQEP) Module > why is Linux on A53 is a NO?? I believe that Nick Saulnier had confirmed Linux drivers for EQEP exists.
Controller Area Network (MCAN) > why not combine CAN & CAN FD rows together? You could then insert a global NO for a CAN XL row.
Timer Modules>
Timers>
Timer -- question - does this row apply apply to hardware in core "dmtimer" modules? Nick Saulnier also confirmed dmtimer support on A53 Linux for me.