This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: How to set up the software when using μSD

Part Number: AM623
Other Parts Discussed in Thread: AM625, SK-AM62B, SK-AM62-LP

Tool/software:

Hi team

When using a μSD (both when booting with the μSD and during normal use),

I think I will need to use GPIO to reset the VSEL_SD terminal of the PMIC (TPS6521902) and

the power supply to the μSD in order to switch the power supply voltage between 3.3V and 1.8V.

How should I set the SDK or driver in this case?

Also, if there is any documentation regarding the settings, please let me know.

SDK:9.2

CPU:AM6232ASGGHAALW

PMIC:TPS6521902

regards

shungo.