Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software:
Dear TI
[First Question]
I developed a project using general hardware C language and register structure variables in CCS 11 or lower.
Can I develop a project using the same hardware C language and register structure variables in CCS 20?
I have a lot of projects from CCS 11 or lower, so I want to know if the software is compatible or supported for use in CCS 20.
[Second question]
I created an independent CCS project by copying source, header, and cmd files to the project folder using ControlSuite in CCS 11 or lower.
I modified and used the source or cmd provided by ControlSuite.
Can I create an independent CCS project by copying source, header, and cmd files using C2000ware in CCS 20?
or do C2000ware and CCS 20 only support driver libraries?
Very important issue, i study about ccs20 and c2000ware and then transfer hardware c style coding sources to driver library style sources.
Best regards, Choi