Tool/software:

While i am connecting to target by using blazer cortex m4 I am getting this error. Can you breif this query.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:

While i am connecting to target by using blazer cortex m4 I am getting this error. Can you breif this query.
Hi,
Our domain expert is currently out-of-office, please expects some delay in response time.
Regards,
Nitika
Hi,
Can you please confirm have you properly initialized the EVM with SBL binaries? Are you able to see the boot logs when the SoC is powered up?
Please refer EVM_FLASH_SOC_INIT
Regards,
Tushar
yes i have intialized EVM with SBL binaries and i can see boot logs, but still the same issue i have got.
Hi Alekhya,
Can you please tell which version of CCS are you using?
Also are you able to see BLAZAR_Cortex_M4F_1 core also after launching the target configuration file?
Regards,
Tushar
Hi Tushar,
I am using 12.6 version of code composer studio, and i am able to see BLAZAR_Cortex_M4F_1 core after launching the target configuration file.
Regads,
Alekhya
Hi Alekhya,
Please connect to the BLAZAR_Cortex_M4F_1 core to run the application. You will not be able to connect to M4F_0 core as it is running the HSM appimage.
Please refer am623-am623-mcu-sdk-cannot-connect-to-blazar-cortex-m4f-0 for details.
Regards,
Tushar