Other Parts Discussed in Thread: AM68A
Tool/software:
I am working with the AM68a TI processor and trying to communicate with the SX1262 LoRa module using SPI. While I can send commands via SPI, I am not receiving the expected responses. I’ve followed the necessary steps to set up SPI communication but am encountering issues with getting valid data from the module.
Hardware Setup:
- AM68a Processor
- SX1262 LoRa Module
- Using SPI for communication, with chip select (CS) and busy (BUSY) pins configured as per the hardware documentation.
Software Setup:
- Python
spidev
library for SPI communication. - SPI device
/dev/spidev0.0
detected, but I am unable to get a valid response from the SX1262 module. - I’ve attempted to reset the module and wake it up using SPI commands, but the responses remain incorrect or empty.
Observations:
-
The SPI device is present (
/dev/spidev0.0
), but thespidev
kernel module is not loaded, as indicated by the following:lsmod | grep spidev
returned no results.- When attempting to load the
spidev
module usingmodprobe spidev
, I received the error:FATAL: Module spidev not found in directory /lib/modules/6.1.80-dirty
.
-
The permissions for the SPI device are restricted to the root user (
crw-------
), and I am currently accessing it using root. -
The response from the module is consistently
0x00
(empty data), which is not expected. The logic analyzer shows data being sent correctly, but the responses from the device are incorrect.
Questions:
- How do I ensure that the
spidev
module is available and properly loaded on my AM68a platform? It seems like the module is missing, but I would appreciate confirmation on how to properly enable it or rebuild the kernel if needed. - Is there a specific configuration or initialization step I might be missing to properly communicate with the SX1262 using SPI?
- Are there any additional diagnostic steps I can take to isolate the issue with the SPI communication?